S32K344 Platform Module Configuration Item Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 Platform Module Configuration Item Issue

3,407件の閲覧回数
chuanlin
Contributor III

When using the tool to configure the Platform module for S32K344, INTx_ How to write the handler name of IRQn, such as ADC0_ IRQn's is Adc_ Sar_ 0_ Is

chuanlin_0-1684128233526.png

 

0 件の賞賛
返信
5 返答(返信)

3,376件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi chuanlin,

IntCtrl_Ip_InstallHandler ipc_shm_hardirq.png

Did you install the SW32K3_IPCF_3.4.0_D2112.exe?(C:\NXP\SW32K3_IPCF_3.4.0_D2112\UserManual.pdf)

ipc_shm_hardirq.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,370件の閲覧回数
chuanlin
Contributor III

chuanlin_0-1684217780461.png

Can IPCF be downloaded normally here?

0 件の賞賛
返信

3,322件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

After reading jiri_kral's reply I realized there should be a newer version of IPCF. 
Sorry for my wrong answer earlier.
Please download lPCF from Real-Time Drivers (RTD), after click DOWNLOAD of S32K3 Standard Software you should be able to see the Automotive SW - S32K3 - Inter-Platform Communication Framework

S32K3 Standard Software DOWNLOAD.pngAutomotive SW - S32K3 - Inter-Platform Communication Framework.png

0 件の賞賛
返信

3,360件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Can you download those two software after click it?

IPCF for S32K3.png

0 件の賞賛
返信

3,373件の閲覧回数
chuanlin
Contributor III

Do EB need to install a new plugin if they want to configure the IPCF module!

0 件の賞賛
返信