S32K344 PIT Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 PIT Config

1,632件の閲覧回数
Yown
Contributor II

When I refer to this example for learning, i get trouble in some variable undeclared

Yown_0-1719646203461.pngYown_0-1719646203461.png

 

Yown_1-1719646233536.pngYown_1-1719646233536.png

i  compare my blank project and example project,  the `Clock_Ip_xxx`missing under /borad

Yown_2-1719646281646.pngYown_2-1719646281646.png

 

and i found template of them

Yown_3-1719646453256.pngYown_3-1719646453256.png

 

so how should i config the project to generate this files successfully?

 

0 件の賞賛
返信
2 返答(返信)

1,571件の閲覧回数
Yown
Contributor II

oh, i got it , i miss "Intctrl_Ip_Init" in main, hardfault is called by the func inside callback, all routine operate suceesful

0 件の賞賛
返信

1,582件の閲覧回数
Yown
Contributor II

Yown_0-1719800059822.pngYown_0-1719800059822.png

Yown_1-1719800079118.pngYown_1-1719800079118.png

Yown_2-1719800153395.pngYown_2-1719800153395.png

 

Now i add mcu module config and update OsIfGeneral, files generated in dir "generate", but siul2 part didn't update successful, is there a reference for the latest edition?

0 件の賞賛
返信