S32K344 14-bit ADC Resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 14-bit ADC Resolution

1,490件の閲覧回数
oskarjohansson
Contributor I

I'm working with the S32K344s ADC. The datasheet and specification on the website states a 12-bit resolution, but the ADC peripheral can be set to 14-bit resolution in the CALBISTREG register. 

What would the difference between the 14-bit resolution and 12-bit resolution be if the ADC is specified to 12-bit?

Best regards,

Oskar Johansson

0 件の賞賛
返信
1 返信

1,475件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Oscar,

The ADC has not been specified at the 14-bit resolution, we don't have any measurements for that.

Even though the TUE should be slightly better at 14bit resolution, because of the lack of data, we can say that If TUE = +/-4 LSB at 12bit, it is +/-16 LSB at 14bit.

 

Best regards,

Daniel

0 件の賞賛
返信