S32K314

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
12,287 Views
youxi
Contributor IV

HI:

The MCU is connected according to the figure below, but simulation is not possible.

 

youxi_2-1692691266949.png

youxi_4-1692691519685.png

 

 

 

youxi_1-1692691175903.png

 

 

Tags (1)
0 Kudos
Reply
1 Solution
12,070 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Do you have any other probe?

I would recommend contacting SEGGER support.

 

Regards,

Daniel

View solution in original post

0 Kudos
Reply
9 Replies
5,280 Views
AmyHuang666
Contributor II

Hi team,

I downloaded bootloader project from this link https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099, and I found the RTD is with AUTOSAR. I would like to use a RTD without AUTOSAR. How can I replace the RTD and where can I download a RTD without AUTOSAR. 

By the way, the chipset is S32K314

Thank you so much~

0 Kudos
Reply
12,269 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @youxi,

What project have you loaded to the MCU? Can you share it?

Can you create a new empty project for S32K314 in S32DS IDE and load it?

 

Thank you,

BR, Daniel

 

 

 

0 Kudos
Reply
12,249 Views
youxi
Contributor IV
Hi.@danielmartynek,
I built an empty project. But there is no way to simulate an empty project
0 Kudos
Reply
12,237 Views
danielmartynek
NXP TechSupport
NXP TechSupport

In you first post, the screenshot indicate that the project was loaded and the execution was halted at a breakpoint in SRAM at 0x2000033C (PC register).

What is the error message now?

Can you share the debug configuration?

Can you place a breakpoint in the startup code (reset routine)?

 

Thank you,

BR, Daniel

 

0 Kudos
Reply
12,144 Views
youxi
Contributor IV

Hi:

The attachment is the result output during S32K314 simulation.

 

Tags (1)
0 Kudos
Reply
12,127 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @youxi,

In the log, I see that the J-link tries to program S32K312.

danielmartynek_0-1693483334147.png

I understand you have S32K314.

This would explain the failure to program it.

 

Regards,

Daniel

0 Kudos
Reply
12,078 Views
youxi
Contributor IV

Hi@danielmartynek 

I changed the device to s32k314, but still can't successfully

Tags (1)
0 Kudos
Reply
12,071 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Do you have any other probe?

I would recommend contacting SEGGER support.

 

Regards,

Daniel

0 Kudos
Reply
12,033 Views
youxi
Contributor IV

Hi @danielmartynek 

The value of the CFSR register is 1.The address that the pc pointer refers to is 0x820E4000. I don't know what error this address represents

youxi_4-1693991411023.pngyouxi_5-1693991430703.png

 

0 Kudos
Reply