S32K314 standby ram usage issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 standby ram usage issues

1,650 Views
SHCHOU
Contributor I

Hello

I setup 32K standby ram in linker_flash.ld 

SHCHOU_0-1720083170868.png

SHCHOU_1-1720083315646.png

SHCHOU_2-1720083364828.png

The set variable are also in relevant memory section

SHCHOU_3-1720083600339.png

and power on will init...

SHCHOU_4-1720084007026.png

 

but standby mode exit , these data not save!?

I don't know why?

there is something wrong with my initialzetion? 

or what steps are missing when entering standby mode?

Please help 

Thank you,

 

0 Kudos
Reply
3 Replies

1,635 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SHCHOU,

Modify the linker file to separate the 32KB standby RAM (0x2040 0000 ~ 0x2040 8000) from int_sram memory region, and place standby .bss and .data or .text sections into the new region as well as adjust the link address symbols for customized initialization during startup as such:

Julin_AragnM_2-1720109511030.png

Also, as a note: CM7 CPU D-Cache MUST be disabled to use the Standby RAM area. Or set the standby RAM (0x2040 0000 ~0x2040 8000) as non-cacheable in MPU configuration.

Julin_AragnM_1-1720109465427.png

Keep in mind that the SRAM contents is invalid after Destructive reset.

Best regards,
Julián

0 Kudos
Reply

1,629 Views
SHCHOU
Contributor I

Thanks for your reply,

I have setup 32K standby RAM (0x2040 0000 ~ 0x2040 8000) , can you help me confirm that the setting are correct?

and i have also setup standby ram as non-cacheable in MPU configuration.

this setting is ok?

SHCHOU_0-1720142851544.png

 

0 Kudos
Reply

1,554 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SHCHOU,

Yes, it should be correct. Keep in mind that the linker file and startup code does not include initialized data to this section. The linker file explicitly mentions that:

Julin_AragnM_0-1720561360881.png

Best regards,
Julián

0 Kudos
Reply