S32K314 LWIP Pack Installtion issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K314 LWIP Pack Installtion issue

ソリューションへジャンプ
2,456件の閲覧回数
YXE
Contributor II

The SW32K3xx_S32DS_3.5.0_D2303.zip have been installed alrady , but i can't find the relate module. And i cannt find the relate examples.

YXE_0-1698745009270.png

YXE_2-1698745103162.png

no middleware in my S32DS

YXE_1-1698745041505.png

I cannt find the TCP/IP examples.

YXE_3-1698745171036.png

relate software version as fllow:

YXE_4-1698745276033.png

 

I think the lwip module haven't been installed successfully, but i don't konw how resolve it

 

 

 

0 件の賞賛
返信
1 解決策
2,410件の閲覧回数
YXE
Contributor II

I reinstalled all the softwares and add the S32K39X pack , the TCP/IP pack can install successfully

 

YXE_0-1698831552280.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,433件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it seems files used are proper one. Try to check if you see stack folder within installation

PetrS_0-1698753675362.png

Maybe you can try to uninstall tcpip stacks you have and install it again following steps given in chapter 6.4 Installation of TCP/IP Stack package over RTD of the stack release note.

BR, Petr

0 件の賞賛
返信
2,411件の閲覧回数
YXE
Contributor II

I reinstalled all the softwares and add the S32K39X pack , the TCP/IP pack can install successfully

 

YXE_0-1698831552280.png

 

0 件の賞賛
返信