S32K312 sending error using Flexio SPI as master node

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 sending error using Flexio SPI as master node

852 Views
victory
Contributor V

1.Development environment:S32DS3.5

2.RTD version:4.0.0

3. Refer to the rtd 2.0.3 routine code, detailed code is attached

4. Expected goals such as 4.1 and 4.2

4.1 MOSI only sends data once, while MISO does not receive data

4.2 MOSI triggers the chip selection pin once for every byte of data sent

5. Actual phenomena such as 5.1, 5.2, 5.3, and 5.4

5.1 MOSI keeps sending data, while MISO keeps receiving data

5.2 MOSI triggers the chip selection pin once every 4 bytes of data sent

5.3 Thumbnails

victory_0-1720765461786.png

 

5.4 Unfolding Diagram

victory_1-1720765482905.png

6.Main. c is as follows

#include "Mcal.h"
#include "Clock_Ip.h"
#include "Siul2_Port_Ip.h"
#include "Siul2_Dio_Ip.h"
#include "IntCtrl_Ip.h"
#include "Flexio_Mcl_Ip.h"
#include "Flexio_Spi_Ip.h"


/* Time to transfer all frame data */
#define TIMEOUT             ((uint32)1000000UL)

static uint8_t data_out[10] = {0x1,0x2,3,4,5,6,7,8,9,10}; /* Transmission buffer. */
static uint8_t data_in[10] = {0,0,0,0,0,0,0,0,0,0}; /* Buffer for receiving. */


#define MASTER_EXTERNAL_DEVICE           (Flexio_Spi_Ip_DeviceAttributes_SpiExternalDevice_0_Instance_0)

int main(void)
{
    uint32_t Counter = 0xFFFFFF;

    /** Clock IPL Init */
    Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);

    /** siul2 pins init */
    Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,\
            g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);

    IntCtrl_Ip_Init(&IntCtrlConfig_0);

    Flexio_Mcl_Ip_InitDevice(&Flexio_Ip_xFlexioInit);

    Flexio_Spi_Ip_Init(&Flexio_Spi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_0);

    /* Update Framesize */
    Flexio_Spi_Ip_UpdateFrameSize(&MASTER_EXTERNAL_DEVICE, 16U);

    /* Update Transfered Bit order */
    Flexio_Spi_Ip_UpdateLsb(&MASTER_EXTERNAL_DEVICE, FALSE);

    Flexio_Spi_Ip_SyncTransmit(&MASTER_EXTERNAL_DEVICE, data_out, data_in, 10, TIMEOUT);

    while (FLEXIO_SPI_IP_IDLE != Flexio_Spi_Ip_GetStatus(MASTER_EXTERNAL_DEVICE.Instance));
}
7.The software related configurations are as follows
7.PIN
victory_2-1720765588032.png

 

7.2flexio_spi

victory_3-1720765644833.png

 

victory_4-1720765666996.png

7.3 flexio_mcl_ip

victory_5-1720765771354.png

 

victory_6-1720765788318.png

 

Above,thanks!

0 Kudos
Reply
0 Replies