S32K312 reset signal pull down problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 reset signal pull down problem

4,436 Views
feiyiniu
Contributor II

During testing, it was found that when S32K312 was in standby mode and the Reset signal was pulled down 0-25ms, the reset reason obtained was wake-up reset: MCU_ WAKEUP_ REASON.And Reset signal are pulled down for 30ms or more, the reset reason obtained is power on reset: MCU_ POWER_ ON_ RESET. May I ask why this situation occurs?Thanks!

0 Kudos
Reply
8 Replies

3,664 Views
JackKai
Contributor I

When using the S32K312 chip, I encountered the following problems. During the entire software OTA process, the data will first be downloaded and verified. After the verification is completed, the Hse area will be cut and the software will be reset. However, occasionally the software cannot be reset and the RST pin of the MCU periodically sends a 50us pull signal at 28ms. Low action.

0 Kudos
Reply

3,665 Views
JackKai
Contributor I

I am encountering a problem now. After the software is downloaded and verified, the software will be reset. After the reset is completed, HSE zone switching will be performed. At this time, zone switching exceptions will occasionally occur, causing the current controller to be abnormal. The RST pin will be abnormal with a 28ms cycle after powering on. Pull low.

0 Kudos
Reply

4,413 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @feiyiniu,

I understand you use the RTD drivers, which version do you use?

Can you please monitor the power supply of the MCU?

If DES[F_POR] = 1, all reset status in the FES and DES registers must be ignored at power up.

Otherwise, can you read the MC_ME[MODE_STAT] and all the MC_RGM registers at the beginning of main()? 

danielmartynek_0-1687248030729.png

 

Thank you,

BR, Daniel

 

0 Kudos
Reply

4,413 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @feiyiniu,

I understand you use the RTD drivers, which version do you use?

Can you please monitor the power supply of the MCU?

If DES[F_POR] = 1, all reset status in the FES and DES registers must be ignored at power up.

Otherwise, can you read the MC_ME[MODE_STAT] and all the MC_RGM registers at the beginning of main()? 

danielmartynek_0-1687248030729.png

 

Thank you,

BR, Daniel

 

0 Kudos
Reply

4,372 Views
feiyiniu
Contributor II

My version is S32K3_RTD_2_0_0_D2203_ASR_REL_4_4_REV_0000_20220331;

The MCU is powered on all the time;

The reset cause is power-on reset: (reset pulse width above 30ms)

MC_ME[MODE_STAT] = 0x0000_0000

MC_RGM[DES] = 0x0000_0001

MC_RGM[FES] = 0x0000_0000

MC_RGM[RDSS] = 0x0000_0000

Power_Ip_GetResetReason() obtain the reset source is MCU_POWER_ON_RESET

The reset cause is wake reset: (reset pulse width 0-25ms)

MC_ME[MODE_STAT] = 0x0000_0000

MC_RGM[DES] = 0x0000_0000

MC_RGM[FES] = 0x0000_0001

MC_RGM[RDSS] = 0x0000_0001

Power_Ip_GetResetReason() obtain the reset source is MCU_WAKEUP_REASON

0 Kudos
Reply

4,354 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @feiyiniu,

This would be the POR_WDG.

danielmartynek_1-1687870380875.png

Please have a look at the RM, Chapter 34 Power-on Reset Watchdog (POR_WDG).

 

Regards,

Daniel

 

 

 

0 Kudos
Reply

4,295 Views
feiyiniu
Contributor II

The POR_WDG configuration is valid in standby mode, but invalid in normal mode. It can be understood that the POR_WDG configuration is only available in standby mode?

Thanks!

0 Kudos
Reply

4,278 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @feiyiniu,

It depends on the DCF record, but by default it is enabled:

danielmartynek_0-1688465772632.png

 

BR, Daniel

 

 

0 Kudos
Reply