S32K312 not programming- Showing Secure Boot Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 not programming- Showing Secure Boot Issue

7,625 Views
sharad_yadav
Contributor III

Dear all, 

Facing issue with programming S32K312. 

Checked all hardware related points on board, all voltages are ok. Connection from Multilink FX to Board programing connector is also ok. 

Error reads as below:

"Secure Debug might be enabled on this device, if so please unlock the device via PEmicro scripts before attempting to connect again (See pemicro.com/securedebug/s32k3 for more information)"

Check attachment as well. 

Request all to check and help. 

 

Regards, 

Sharad

0 Kudos
Reply
7 Replies

7,091 Views
SethWang
NXP Employee
NXP Employee

Hi,

My customer met the same issue.

How to solve it?

BR,

Seth

0 Kudos
Reply

7,086 Views
sharad_yadav
Contributor III
@SethWang Not able to solve this issue. Chip was locked in production itself. Get new samples from NXP and then check. FYI: We moved to another chip manufacturer for this project.
0 Kudos
Reply

7,082 Views
SethWang
NXP Employee
NXP Employee

Hi sharad_yadav,

Got it.

Thanks a lot.

BR,

Seth

0 Kudos
Reply

7,601 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @sharad_yadav,

Can you please follow the instructions from this link pemicro.com/securedebug/s32k3 ?

 

BR, Daniel

 

0 Kudos
Reply

5,591 Views
abunayeeem
Contributor II

@danielmartynek 

In one of out custom control card, we are also facing the same issue. 
we are encountering the following error:

"Secure Debug might be enabled on this device. If so, please unlock the device via PEmicro scripts before attempting to connect again."

abunayeeem_0-1733585616588.jpeg



could you please suggest us a solution for this?



Tags (1)
0 Kudos
Reply

7,332 Views
PatrickPP1
Contributor I

HI!

In this link "pemicro.com/securedebug/s32k3 ",The second py script should input a key, but this key should be registed by the nxp smart card. I do not have the NXP smart card ,Please help me to solve this problem ,thanks a lot. 

Patrick

0 Kudos
Reply

5,587 Views
abunayeeem
Contributor II

Hi @PatrickPP1, 
did you manage to authenticate the debugger or unlock the secure debug mode? 

0 Kudos
Reply