S32K312 not programming- Showing Secure Boot Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 not programming- Showing Secure Boot Issue

7,815件の閲覧回数
sharad_yadav
Contributor III

Dear all, 

Facing issue with programming S32K312. 

Checked all hardware related points on board, all voltages are ok. Connection from Multilink FX to Board programing connector is also ok. 

Error reads as below:

"Secure Debug might be enabled on this device, if so please unlock the device via PEmicro scripts before attempting to connect again (See pemicro.com/securedebug/s32k3 for more information)"

Check attachment as well. 

Request all to check and help. 

 

Regards, 

Sharad

0 件の賞賛
返信
7 返答(返信)

7,281件の閲覧回数
SethWang
NXP Employee
NXP Employee

Hi,

My customer met the same issue.

How to solve it?

BR,

Seth

0 件の賞賛
返信

7,276件の閲覧回数
sharad_yadav
Contributor III
@SethWang Not able to solve this issue. Chip was locked in production itself. Get new samples from NXP and then check. FYI: We moved to another chip manufacturer for this project.
0 件の賞賛
返信

7,272件の閲覧回数
SethWang
NXP Employee
NXP Employee

Hi sharad_yadav,

Got it.

Thanks a lot.

BR,

Seth

0 件の賞賛
返信

7,791件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @sharad_yadav,

Can you please follow the instructions from this link pemicro.com/securedebug/s32k3 ?

 

BR, Daniel

 

0 件の賞賛
返信

5,781件の閲覧回数
abunayeeem
Contributor II

@danielmartynek 

In one of out custom control card, we are also facing the same issue. 
we are encountering the following error:

"Secure Debug might be enabled on this device. If so, please unlock the device via PEmicro scripts before attempting to connect again."

abunayeeem_0-1733585616588.jpeg



could you please suggest us a solution for this?



タグ(1)
0 件の賞賛
返信

7,522件の閲覧回数
PatrickPP1
Contributor I

HI!

In this link "pemicro.com/securedebug/s32k3 ",The second py script should input a key, but this key should be registed by the nxp smart card. I do not have the NXP smart card ,Please help me to solve this problem ,thanks a lot. 

Patrick

0 件の賞賛
返信

5,777件の閲覧回数
abunayeeem
Contributor II

Hi @PatrickPP1, 
did you manage to authenticate the debugger or unlock the secure debug mode? 

0 件の賞賛
返信