S32K312 how to open CAN_example_CT.mex with correct S32DS version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 how to open CAN_example_CT.mex with correct S32DS version

494件の閲覧回数
PINKMAN
Contributor III

my S32DS version is V3.5, and my chip is S32K312, RTD version is SW32K3_RTD_4.4_2.0.0, i import the example Can_example_S32K312.when open the .mex file ,it report a error as below. i want to know which version of RTD i can used for S32DS3.5,because i want to study  can cfg in S32K312

AC680753-7586-4c13-86D2-A94E1297807D.png

08B11AE1-A684-46c1-B5B0-F21B96B34876.png

0 件の賞賛
返信
1 返信

470件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @PINKMAN,

If you are using S32DS, you should use the "S32DS" folder instead of the EBT, those examples are for the EB Tresos platform.

Julin_AragnM_0-1725036169781.png

You can also use the S32DS Project from Example option:

Julin_AragnM_3-1725036318127.png

Best regards,
Julián

0 件の賞賛
返信