S32K312 debug port disable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 debug port disable

2,421 Views
Yiming2
Contributor III

hello

I am try to completely/permanently disable the debug port. and I also find the following content in HSE_B manual(latest version).

Yiming2_1-1714270892190.png

Yiming2_0-1714270777671.png

but I did not find any more description in RM or HSE_B. So how to completely disable the debug port?

Tags (1)
0 Kudos
Reply
4 Replies

1,699 Views
Juan_Gonzalez1
Contributor I

I have the same question for MCWT2xxxS, is it posible to disable debug port?

0 Kudos
Reply

1,680 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Juan_Gonzalez1 

MCWT2xxxS is a derivative of S32K312, so the answer is the same:  it's not possible to disable the debug completely.

Regards,

Lukas

0 Kudos
Reply

1,664 Views
Juan_Gonzalez1
Contributor I

Thanks Lukas, The MCWT2xxxS Reference manual mentions that the details of security feature are in Security Reference Manual, Can you provide me that document or any other reference for debug protection implementation please?

0 Kudos
Reply

2,391 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Yiming2 

it's not possible to disable the debug port completely on this device. The only option is to use static or dynamic protection of the debug port (i.e. password or key). There's already a request to remove all references to "debug disable" from the HSE FW RM.

Regards,

Lukas

0 Kudos
Reply