Hello,
I am using an S32K312 MCU and have run out of SRAM (>32KB).
Hareesh_S_0-1754913458015.png
From my understanding, the K312 has 96KB of SRAM, where 32KB is standby RAM, 32KB is no_cacheable and the last 32KB is shareable.
I do not fully understand the practical limitation to these sections, specifically with respect to the shareable section, given that the K312 is a single core and non-lockstep MCU. (I assume no_cacheable implies that data here cannot be moved to cache?)
Is there a section of the reference manual I should refer to for more information on this? All I have found is AN13388 but it only seems to describe the standby section in detail.
Additionally, what are int_sram_fls_rsv, int_sram_results and int_stack_dtcm sections for?
Tying back to my initial problem, if I am using more than 32KB ram (statically) do I need to manually place certain variables in the other ram sections? And how does this behaviour change WRT stack/heap? Can my stack/heap grow more than 32KB?
Much thanks in advance!