S32K312 - Multiple ADC conversion read with DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K312 - Multiple ADC conversion read with DMA

跳至解决方案
4,032 次查看
BRK_Y
Contributor III

Hi everyone,

I need to read 4 ADC channels. Two of them are ADC-0 and the other two are ADC-1 channels.

I configured BCTU, PIT, and TRGMUX to ensure continuous conversion.

I want the conversion results to be stored in the buffer I specified with DMA.

Created a list to start the conversion of ADC channels with a single BCTU trigger.

I want to ask here:

Do I need to create four DMA channels for four ADC channels?

Can't I get the result of four ADC channels with a single DMA channel? 

0 项奖励
回复
1 解答
3,755 次查看
PetrS
NXP TechSupport
NXP TechSupport
4 回复数
3,953 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there is no need to have 4 DMA channels for 4 ADC results. You can configure a list to perform 2 parallel conversions. Refer to chapter 65.3.4 Multiple parallel conversions (MPC) of the RM. 
If the DATA_DEST of the trigger selects one of the FIFO, you can read 4 converted results from that selected FIFO using single DMA channel (watermark set to 3).
I put some PIT BCTU ADC DMA example at https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/... but BCTU data register is set as result destination so it would need some modification to follow your need.

BR, Petr

0 项奖励
回复
3,901 次查看
BRK_Y
Contributor III

Hi @PetrS,

Thank you for your answer, but my problem persists. I cannot get the ADC conversion result in the buffer I gave to the BCTU unit.

Let me briefly explain what I did.

I configured ADC-0 and ADC-1:

ADC0-1_cfg.png

And also i configured related channels

ADC-0:

adc_0_ch_cfg.png

ADC-1:

adc_1_ch_cfg.png

BCTU configurations:

bctu_hw_unit_1.png

bctu_hw_unit_2.png

TRGMUX and PIT configurations:

trgmux_cfg.png

pit_cfg.png

DMA configurations:

dma_Cfg.png

Even though I made all these configurations, no data is written to the buffer I gave to DMA.

When I check FIFODR1 with debug, I see the data, but FIFO does not run DMA for some reason.

When I reviewed the driver functions, I saw that bctu turns off the DMA hardware request every time the transfer ends in DMA configurations.

To prevent this, the function named Bctu_Ip_FifoDmaHandler is called within the Bctu_Ip_Bctu0Fifo1DmaComplete function. Thus, the DMA hardware request is refreshed.

BrK__0-1695492694785.png

What I want to ask here is who calls the Bctu_Ip_Bctu0Fifo1DmaComplete function and when. Could it be related to my problem?

What am I missing so that DMA can work and an interrupt occurs in the DMA major loop?

0 项奖励
回复
3,756 次查看
PetrS
NXP TechSupport
NXP TechSupport
4,012 次查看
justoxy
Contributor I

Hello!
I have similar setup (but with s32k311 and three ADC channels on a single instance) and related question. I am trying to have BCTU trigger DMA transfer of FIFO1 conversion results and then DMA to trigger interrupt. None of this happens - BctuDmaFifo1 is empty and no interrupt from dma. With BCTU interrupt notification it works correctly.
P.S. DMA Global/transfer config is disabled because I can see that it's set in Bctu_FifoSetupDma().
Can you tell me please what I might be missing here?
bctu_dma_config.PNG

0 项奖励
回复