S32K312+FS26 watchdog refresh

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312+FS26 watchdog refresh

1,507 Views
Akhil1
Contributor I

Hello,

I am working on S32K312 to do SBC FS26 watchdog refresh every 50 ms. I am facing the issue with the InitDevice function, while Initializing the SBC.

Can anyone help me out?

0 Kudos
Reply
2 Replies

1,494 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Akhil1,

I hope all is great with you. Thank you for using the NXP communities.

As we know, after power up, wake up from Standby or RSTB assertion, the fail-safe state machine is moving through several states and wait in Init_FS state. In this state, the RSTB pin is released to high level and the MCU must configure FS_I_xxx registers and then perform a good watchdog refresh within 256 ms.

Do you mean that you are not able to perform the first good watchdog refresh?

diazmarin09_0-1707254584881.png

 

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,486 Views
Akhil1
Contributor I

I solved the problem...Thank you

0 Kudos
Reply