S32K312 FEE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 FEE

1,445件の閲覧回数
fengba_360
Contributor III

Hello, I'm encountering an issue with the FEE initialization process on the s32k312. My program seems to be stuck at the Fee_MainFunction(), preventing me from proceeding with further operations. I've attached my project code. Could you kindly review it for me?

微信图片_20240923230135.png微信图片_20240923230143.png

0 件の賞賛
返信
2 返答(返信)

1,393件の閲覧回数
fengba_360
Contributor III

I'm still waiting for your reply. I might have forgotten to upload the project code before.

0 件の賞賛
返信

1,351件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

I imported your project to S32DS and I can see following error message in the configurator:

***
Issue: The total size of blocks is too big. They do not fit into the cluster group FeeClusterGroup_0. Increase the size of the cluster or reduce the size of blocks.
Level: Error
Type: Tool problem
Tool: Peripherals
Origin: Peripherals
Resource: Sources
Information: The total size of blocks is too big. They do not fit into the cluster group FeeClusterGroup_0. Increase the size of the cluster or reduce the size of blocks.
***

So, you need to reduce FeeBlockSize (I can see in FeeBlockConfiguration_2 that FeeBlockSize is 7168) or you need to increase the size of cluster. The size of cluster can be increased by adding another FeeSubAddressArea. 

I believe that it will work as expected if you fix this error as described above.

lukaszadrapa_3-1727782560039.pnglukaszadrapa_4-1727782567023.pnglukaszadrapa_5-1727782573370.png
 
 

 

0 件の賞賛
返信