S32K312-Error impact when entering StandBy process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312-Error impact when entering StandBy process

1,139 Views
Simon-Liu
Contributor V

Hello

When calling the function Power_Ip_SetMode to enter the StandBy process, there are several timeouts. For example, after setting the PRTN_PCONF register, it will wait for the status change of the PRTN_STAT register. If these timeouts occur, will the S32K312 be unable to enter StandBy and cannot wake up?

 

BestRegards

Simon

0 Kudos
Reply
1 Reply

1,107 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Simon-Liu 

In the following post are provided some examples developed based on RTD/HLD related to low power management, which you can use as a reference. 

 

B.R.

VaneB

0 Kudos
Reply