S32K312 - ADC Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 - ADC Problem

ソリューションへジャンプ
2,570件の閲覧回数
ssean
Contributor IV

Hello.

I have problem with use S32K312, ADC0_S9

I read below articles.

https://community.nxp.com/t5/S32K/S32K344-ADC-HAS-ADC-INTERLEAVE-problem/m-p/1548855

https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680

My RTD version is 2.0.1 (Released 7, July, 2022).

Which RTD version fixed that problem?

 

Best Regards

0 件の賞賛
返信
1 解決策
2,554件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

As I know this bug should be fixed in RTD_4.7_S32K3XX_3.0.0_CD04. But I did not install this version. I have install a new version S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can see that Siul2_Port_Ip_WriteDCMConfiguration has changed. 

Siul2_Port_Ip_WriteDCMConfiguration S32K3 RTD3.0.0 P07.png

By the way, those S32K3 RTD 3.0.0 should be installed in S32DS v3.5. That means you need to install S32DS v3.5 instead of updating RTD in v3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,555件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

As I know this bug should be fixed in RTD_4.7_S32K3XX_3.0.0_CD04. But I did not install this version. I have install a new version S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can see that Siul2_Port_Ip_WriteDCMConfiguration has changed. 

Siul2_Port_Ip_WriteDCMConfiguration S32K3 RTD3.0.0 P07.png

By the way, those S32K3 RTD 3.0.0 should be installed in S32DS v3.5. That means you need to install S32DS v3.5 instead of updating RTD in v3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,537件の閲覧回数
ssean
Contributor IV

Dear @Robin_Shen 

Thank you for your reply.

I'll check that version.

 

Best Regards,

Sean Sung

 

0 件の賞賛
返信