S32K311_48LQFP - ADC mux output channel configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K311_48LQFP - ADC mux output channel configuration

392 次查看
truptikavadi1
Contributor I

Hi,

I have to configure ADC1_MA[0] signal whose pin number is PTB2. For this signal it is given as ADC Mux Output.

1. Can I know which register to be used to read ADC raw data. 

2. May I know the steps to configure this channel.

3. What is the channel number for the above mentioned ADC signal.

0 项奖励
回复
1 回复

353 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I gave general feedback on https://community.nxp.com/t5/S32K/S32K311-LQFP-ADC-Mux-Output-channel-configuration/m-p/2117423/high...

But in case of 48LQFP package there is only one mux output signal MA[0] and one external input X0 on ADC1. So external analog mux cannot be used at all.

PetrS_0-1750163339109.png

You can connect external analog signal to X0 input and this will be measured if external channels 64 to 71 will be selected for conversion. results will be read from CDR64 to 71 depending channel selected.

BR, Petr

0 项奖励
回复