S32K3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3

757件の閲覧回数
yy12
Contributor II

Application consultation about S32K314NHT1VPBST product
I used two batches of chips here (DC2322 and DC24+).
After using the DC24+chip, the static current is only 80uA.
But I found that the static current of the DC2322 batch of chips exceeded the standard, reaching 280uA.
I want to confirm why this is? Is there a difference between two different batches of chips? Or would circuit design lead to the existence of such differences?

タグ(1)
0 件の賞賛
返信
0 返答(返信)