Read a key from secure NVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read a key from secure NVM

2,651 Views
shravani
Contributor II

Hi, I wanted to read a key from secure NVM, is it possible to read back a key? I want to use this key further in my application. I checked the RTD firmware there is only one service for exporting key from RAM. Also, in the Firmware reference manual of HSE it is mentioned that SHE NVM keys cannot be exported. How could I use stored key in my application?

Please check below details.

1) Microcontroller: S32K312_100MQFP

2) IDE: S32DS 3.5  

3) SDK Version: PlatformSDK_S32K3_2022_03

 

shravani_0-1713953011681.pngshravani_1-1713953028240.png

 

0 Kudos
Reply
4 Replies

1,748 Views
HaiHoangSoftware
Contributor IV
 

Hi,

I can not read AES key after import. I'm using NVM key handle.

Importing key is success. But export key is failed.

Is there anyone know how to solve this issue?

Thanks a lot.

Here is my implementation:

hseKeyInfo_t keyInfo = {0};
uint8_t sharedSecret[448];
uint16_t sharedSecretLen = 32;
void testFunction(void) {
hseSrvResponse_t hseResponse = HSE_SRV_RSP_GENERAL_ERROR;
hseResponse = ExportPlainSymKeyReq( EXAMPLE_NVM_KEY_HANDLE,
&keyInfo, sharedSecret, &sharedSecretLen);
}

0 Kudos
Reply

2,623 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is stated in section
6.3.6.2 SHE key update policies

"When RAM_KEY is updated with the SHE key update protocol, it cannot be exported, until it is updated in plain via the key import service or via the SHE plain key update."

"NVM SHE keys cannot be exported." as you already screenshot.

0 Kudos
Reply

2,619 Views
shravani
Contributor II

Hi, I want to apply AES 128 encryption on the key which is stored in the secure NVM. How could I achieve this?

0 Kudos
Reply

2,567 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It cannot be done as a key stored in the secure NVM cannot be exported.

0 Kudos
Reply