S32K3 _Whether RAM data is retained after destructive reset?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 _Whether RAM data is retained after destructive reset?

Jump to solution
2,497 Views
wuxianlong
Senior Contributor I

Hi,all

In my opinion, if it were not for the POR and Standby modes, the data in the RAM should be retained in the destructive reset. The data was also retained in our tests.
We need to use destructive reset, but the manual describes functional reset retention, so we're not sure if there's a risk.

wuxianlong_0-1702889610108.png

Best Regards,
xianlong

 

 

0 Kudos
Reply
1 Solution
2,482 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, they are not.

davidtosenovjan_0-1702919158000.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,483 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, they are not.

davidtosenovjan_0-1702919158000.png

 

0 Kudos
Reply
2,455 Views
wuxianlong
Senior Contributor I

@davidtosenovjan 

    Thank you for you help。
    In the startup.s of RTD4,0,0, initializing standby RAM is determined by whether it is POR or not. If the manual description is correct, is this operation risky?

wuxianlong_0-1703044240194.png

BRs,
xianlong

 

 

0 Kudos
Reply