S32K3 SPD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 SPD

858 Views
Neo1096
Contributor III

Hello.

I use RTD400 and SPD105, and the development board is the S32K312 144P development board

I added the uart module to the tested SPD module (including RAM and flash injection errors) program, and it worked normally. Then I added other modules. (Currently, only the DMA part has been tested, and adding only uart seems to be fine.) Without making any Settings, even if the header file is not referenced in the code, The program will also be in the function Clock_Ip_SetWaitStates(); Then it enters a hardware error interrupt.

I uploaded the code of the FCCU module without adding DMA, and it can run normally. However, after adding it, the clock initialization program hardware error occurs. What could be the reason for this and how can this problem be solved?

0 Kudos
Reply
1 Reply

830 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Neo1096

Please follow your duplicated question:

https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214

 

0 Kudos
Reply