S32K3 SPD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 SPD

860 次查看
Neo1096
Contributor III

Hello.

I use RTD400 and SPD105, and the development board is the S32K312 144P development board

I added the uart module to the tested SPD module (including RAM and flash injection errors) program, and it worked normally. Then I added other modules. (Currently, only the DMA part has been tested, and adding only uart seems to be fine.) Without making any Settings, even if the header file is not referenced in the code, The program will also be in the function Clock_Ip_SetWaitStates(); Then it enters a hardware error interrupt.

I uploaded the code of the FCCU module without adding DMA, and it can run normally. However, after adding it, the clock initialization program hardware error occurs. What could be the reason for this and how can this problem be solved?

0 项奖励
回复
1 回复

832 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Neo1096

Please follow your duplicated question:

https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214

 

0 项奖励
回复