S32K3 RTD ModuleID information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 RTD ModuleID information

ソリューションへジャンプ
1,769件の閲覧回数
sobo
Contributor III

Hello,

 

I would like to know if a list of the ModuleID use by the RTD (S32K3) exist ?
(configurationCommonPublishedInformation/ModuleId )

 

I would like to used Std_ReturnType Det_ReportError(uint16 ModuleId, uint8 InstanceId, uint8 ApiId, uint8 ErrorId) function for RTD and also for some application software.

I would like to have a different ID than those used by RTD drivers for my application

Sophie

タグ(2)
0 件の賞賛
返信
1 解決策
1,752件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi Sobo,

There is no list of the MODULE_ID used by the RTD (S32K3).

From my point of view, you can try to change the MODULE_ID in the RTD driver and test that.

Best regards,

Dan

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,753件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi Sobo,

There is no list of the MODULE_ID used by the RTD (S32K3).

From my point of view, you can try to change the MODULE_ID in the RTD driver and test that.

Best regards,

Dan

 

 

0 件の賞賛
返信