AN5320 soft

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN5320 soft

1,168件の閲覧回数
lengrudie
Contributor III

How can I fine AN5320 demo?

0 件の賞賛
返信
1 返信

1,156件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lengrudie,

There is no Using LPSPI on KL28Z  AN5320SW, so you can not find it. The code is shown in this AN.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信