S32K3 Qspi's bug caused a timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Qspi's bug caused a timeout

ソリューションへジャンプ
2,122件の閲覧回数
wuxianlong
Senior Contributor I

Hi,all

Because the following macro definitions are only defined in S32K344.(QuadSPI_DLLSR_SLVA_LOCK_MASK,QuadSPI_DLLSR_DLLA_LOCK_MASK,QuadSPI_DLLSR_DLLA_RANGE_ERR_MASK) 
So when I use S32K314 or S32K324, Qspi will have logic errors in RTD versions 3.0.0 and 4.0.0.

For example, I call Qspi_Ip_ControllerInit ()-> Qspi_Ip_ConfigureDLL ()-> Qspi_Ip_ConfigureDLLA ()-> Qspi_Ip_ConfigureDLLAByPass ()-> Qspi_Ip_WaitDLLASlaveLock ().
Because the macro is not defined, API returns false. The Qspi_Ip_WaitDLLASlaveLock () waits until a timeout error occurs.

How should I modify it to make QSPI available. Do I add my own macro definition?

wuxianlong_1-1709541309865.png


wuxianlong_0-1709539634022.png

BRs,
xianlong

0 件の賞賛
返信
1 解決策
2,074件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @wuxianlong 

We have verified the situation you mentioned. At this moment, the workaround we can provide is to copy the missing declarations and the structure parameters from the S32K344 header to the S32K324 and S32K314. 

This situation has already been reported to the corresponding team, and we expect it to be solved in future software revisions. 

Sorry for all the inconvenience caused.

 

B.R

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,075件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @wuxianlong 

We have verified the situation you mentioned. At this moment, the workaround we can provide is to copy the missing declarations and the structure parameters from the S32K344 header to the S32K324 and S32K314. 

This situation has already been reported to the corresponding team, and we expect it to be solved in future software revisions. 

Sorry for all the inconvenience caused.

 

B.R

VaneB

0 件の賞賛
返信