S32K3 LPCMP module Latency issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 LPCMP module Latency issues

8,768 Views
yinq
Contributor I

Hi,

I have encountered some problem of S32K3 , LPCMP module.

yinq_0-1682502183212.png

Which position may Tper appear in A, B, C, D, and indicate the number of Tper in this position?

0 Kudos
Reply
11 Replies

8,683 Views
zhanguiyang
Contributor I

How to handle the cross clock domain transition from window function to filter when using mode # 4A? Because in # 4A mode, the signal input to the filter is asynchronous with the filter clock window/sample.

0 Kudos
Reply

8,685 Views
zhanguiyang
Contributor I

How to handle the cross clock domain transition from window function to filter when using mode # 4A? Because in # 4A mode, the signal input to the filter is asynchronous with the filter clock window/sample.

0 Kudos
Reply

8,670 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

If CCR1[SAMPLE_EN] is set to 1, the low-pass filter samples COUTA on each positive transition of the sample/window input. Window signal must be of minimum 4 bus cycle pulse for window mode to function. The output state of the filter changes when all the consecutive CCR1[FILT_CNT] samples agree that the output value has changed.

BR, Petr

0 Kudos
Reply

8,478 Views
zhanguiyang
Contributor I

When CCR1[SAMPLE_EN]=1, the window/sample signal acts as the clock of the filter, asynchronously with the bus clock?

If they are asynchronous, can window/sample signals count against COUTA directly?

0 Kudos
Reply

8,456 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

If CCR1[SAMPLE_EN] is set to 1, at positive transition of the sample/window signal COUTA is sampled and filter counts specifies the number of consecutive samples that must agree before the comparator output filter accepts the sample as a new valid output state.

BR, Petr

0 Kudos
Reply

8,441 Views
zhanguiyang
Contributor I

So,is the working clock of the filter a bus clock? window_sample signal is not the working clock of the filter?

0 Kudos
Reply

8,412 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is a feedback I got from Apps team.

When CCR1[SAMPLE_EN]=1, the window/sample signal acts as the clock of the filter, asynchronously with the bus clock? 

Yes

If they are asynchronous, can window/sample signals count against COUTA directly?

I can understand your mean. But you can refer the attachments which include the detail of filter, sample and window.

So, is the working clock of the filter a bus clock? Window_sample signal is not the working clock of the filter?

The LPCMP working clock of the filter is bus clock. Window_sample signal is the sample input and is not the working clock of the filter.

 

BR, Petr

0 Kudos
Reply

8,645 Views
zhanguiyang
Contributor I

In 4A mode, such as filt_ cnt=5,couta is output by the bus clock.but,when couta go in filter, the clock of the filter at this time is asynchronous window/sample signal. The first sampling count of couta by window/sample may have metastable state,How to solve this problem?

0 Kudos
Reply

8,584 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

in this mode, the path from the analog inputs to COUTA is combinational (unclocked). COUTA is then input to Filter and COUT is sampled signal. A first sample will always happen at uncertain time and can be from 0 to period of sampling signal. This cannot be influenced anyhow.

BR, Petr

0 Kudos
Reply

8,739 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there will be 2 Tper clock synchronization in the Window function (point B) and ((CCR1[FILT_CNT] x CCR1[FILT_PER]) + 1) x Tper clock for the Filter function (point D).

BR, Petr

0 Kudos
Reply

8,692 Views
zhanguiyang
Contributor I
How to handle the cross clock domain transition from window function to filter when using mode # 7?
0 Kudos
Reply