S32K3 Firmware Update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Firmware Update

ソリューションへジャンプ
2,482件の閲覧回数
DiaDev
Contributor III

Hello,

Could you please provide the S32K3XX Firmware Update Application Note, similar to the S32K1XX Firmware Updates Application Note (AN12323: S32K1xx Firmware updates – Application Note)?

It would be greatly appreciated!

Thanks !.

1 解決策
2,452件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DiaDev

There is no direct application note for the S32K3XX devices as with the S32K1XX; However, there are some ANs and examples for FW updates:

Under the S32K3 HSE Demo Examples, there is the Secure boot & Device configuration examples, which showcase basic/advanced secure boot, HSE installation (FULL_MEM & AB SWAP), along with other functionalities.

There is also the OTA DEMO application which can be found in S32K3 Reference Software: SW32K3-REFSW-D.

Finally, you can also refer to the Unified bootloader Demo & the Example S32K312 Bootloader to Application Jump DS3.5 RTD300 from the community.

Hope this helps & best regards,
Julián

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,453件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DiaDev

There is no direct application note for the S32K3XX devices as with the S32K1XX; However, there are some ANs and examples for FW updates:

Under the S32K3 HSE Demo Examples, there is the Secure boot & Device configuration examples, which showcase basic/advanced secure boot, HSE installation (FULL_MEM & AB SWAP), along with other functionalities.

There is also the OTA DEMO application which can be found in S32K3 Reference Software: SW32K3-REFSW-D.

Finally, you can also refer to the Unified bootloader Demo & the Example S32K312 Bootloader to Application Jump DS3.5 RTD300 from the community.

Hope this helps & best regards,
Julián

 

0 件の賞賛
返信