S32K3 FLASH write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 FLASH write

跳至解决方案
2,126 次查看
DouDou1
Contributor III

Hi, everyone

I am using the first core of the S32K358 chip to program, I want to put the BOOTLOADER program in the memory of PFLASH0, and then put the APP program in the memory of PFLASH1, can the APP run properly?

0 项奖励
回复
1 解答
2,066 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

It doesn't matter which master accesses a flash block.

There's simple rule - if a block is being erased or programmed, it's now allowed to access this block. Only other blocks can be accessed at that time.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,092 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @DouDou1 

Yes, there's no problem with this setup. There are four code flash blocks and read-while-write is supported between these blocks.

Regards,

Lukas

0 项奖励
回复
2,080 次查看
DouDou1
Contributor III

Hi,@lukaszadrapa,
Thank you for your reply, I want to know if the first core of the S32K358 chip can read-while-write all four code?

0 项奖励
回复
2,067 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

It doesn't matter which master accesses a flash block.

There's simple rule - if a block is being erased or programmed, it's now allowed to access this block. Only other blocks can be accessed at that time.

Regards,

Lukas

0 项奖励
回复
2,054 次查看
DouDou1
Contributor III
Thank you for your reply.
0 项奖励
回复