S32K3 ECC error detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 ECC error detection

2,551件の閲覧回数
DGB
Contributor II

Hi,

I have a question in terms of single/double-bit error detection. Taking into account following statement from S32K3 RM my understanding is that for DFLASH and PFLASH there is possibility to detect only double bit failure, since single bit errors are automatically corrected. Is this correct understanding?  

DGB_0-1733819222203.pngDGB_0-1733819222203.png

What registers should be taken into account in order to detect double-bit errors for DFLASH and PFLASH?

 

0 件の賞賛
返信
3 返答(返信)

2,486件の閲覧回数
DGB
Contributor II

Thank you for the response. So in order to detect any single or double bit errors  on DFLASH and PFLASH it would be sufficient to pull MCRS[SBC] and MCRS[EER] values periodically during runtime? 

0 件の賞賛
返信

2,478件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DGB,

This is question on functional safety.

Refer to the S32K3xx Safety Manual or ask in the SafeAssure community

https://community.nxp.com/t5/SafeAssure-Community/gh-p/52177

 

Regards,

Daniel

0 件の賞賛
返信

2,521件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DGB,

The Error Reporting Module (ERM) can detect single-bit errors on the Flash memory too.

danielmartynek_0-1733907048737.pngdanielmartynek_0-1733907048737.png

And the Embedded Flash Memory (c40asf) also informs about single-bit errors.

Module Configuration Status (MCRS[SBC]).

danielmartynek_1-1733907130872.pngdanielmartynek_1-1733907130872.png

 

Regards,

Daniel

0 件の賞賛
返信