S32K3 ECC error detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 ECC error detection

2,625 Views
DGB
Contributor II

Hi,

I have a question in terms of single/double-bit error detection. Taking into account following statement from S32K3 RM my understanding is that for DFLASH and PFLASH there is possibility to detect only double bit failure, since single bit errors are automatically corrected. Is this correct understanding?  

DGB_0-1733819222203.png

What registers should be taken into account in order to detect double-bit errors for DFLASH and PFLASH?

 

0 Kudos
Reply
3 Replies

2,560 Views
DGB
Contributor II

Thank you for the response. So in order to detect any single or double bit errors  on DFLASH and PFLASH it would be sufficient to pull MCRS[SBC] and MCRS[EER] values periodically during runtime? 

0 Kudos
Reply

2,552 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DGB,

This is question on functional safety.

Refer to the S32K3xx Safety Manual or ask in the SafeAssure community

https://community.nxp.com/t5/SafeAssure-Community/gh-p/52177

 

Regards,

Daniel

0 Kudos
Reply

2,595 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DGB,

The Error Reporting Module (ERM) can detect single-bit errors on the Flash memory too.

danielmartynek_0-1733907048737.png

And the Embedded Flash Memory (c40asf) also informs about single-bit errors.

Module Configuration Status (MCRS[SBC]).

danielmartynek_1-1733907130872.png

 

Regards,

Daniel

0 Kudos
Reply