S32K3 DMAMUX channel assignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 DMAMUX channel assignment

ソリューションへジャンプ
2,440件の閲覧回数
mnovaro
Contributor I

 

In the S32K3 Reference Manual, I can read:

DMAMUX_0 and DMAMUX_1 channels are mapped to eDMA_TCD 0–5 and 6–12, respectively.

This can be valid for S32K312, which includes 12 TCD descriptors.

As far as I can see, any other S32K device (S32K322/S32K342/S32K314/S32K324/S32K344) has 32 TCD in total, and in fact it also has 16 channels per DMAMUX instance. In all these devices, which is the mapping between the DMAMUX channel and the TCD? Is it simply 1:1 ?

DMAMUX_0 - TCD0-15

DMAMUX_1 - TCD16-31

Thank you for your feedback

 

0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you are right. It should be stated that

DMAMUX_0 and DMAMUX_1 channels are mapped to eDMA_TCD 0–15 and 16–31, respectively.

excluding S32K312 where

DMAMUX_0 and DMAMUX_1 channels are mapped to eDMA_TCD 0–5 and 6–12, respectively.

 

Thank you for your findings. I will report it as documentation bug.

元の投稿で解決策を見る

1 返信
2,429件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you are right. It should be stated that

DMAMUX_0 and DMAMUX_1 channels are mapped to eDMA_TCD 0–15 and 16–31, respectively.

excluding S32K312 where

DMAMUX_0 and DMAMUX_1 channels are mapped to eDMA_TCD 0–5 and 6–12, respectively.

 

Thank you for your findings. I will report it as documentation bug.