S32K3 ADC Filter Capacitance Selection Range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 ADC Filter Capacitance Selection Range

1,961 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

On S32K3 Data Sheet, Figure 33 [SAR ADC Input Circuit].

SAR ADC Input Circuit.jpg

Could you please clarify the Filter Capacitance (CF) selection range. Is there any formula for this value?

Ps: S32K312 MCU Clock: 120 MHz, ADC clock speed: 80 MHz

 

BR,

Hornby

0 Kudos
Reply
1 Reply

1,950 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The C_F is related to the RC filter (or low pass filter) intended for the ADC input to have, in order to reduce the noise that will input the ADC pin.

The selection of both R_F and C_F is mainly related to the cut-off frequency that it is needed to reduce unwanted noise on the ADC input. The formula can be the one shown below:

DanielAguirre_0-1678904130217.png

Please, let us know if this information was helpful or not.

0 Kudos
Reply