Trace, Debug, Bist , S32K , Functional Reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trace, Debug, Bist , S32K , Functional Reset

2,417 Views
Higgs_Boson
Contributor I

Hi, Teams,

We are using BIST in the s32k project,  Since bist will cause functional reset after test done. And

1. we wonder how to use debug tool(e.g. trace32) to trace the software when s32k is performed a functional reset.

2. and, how to reinit s32k after functional reset .because I notice the ram is become "???" after the functional reset: 

Higgs_Boson_0-1678782750692.png

Thanks.

0 Kudos
Reply
3 Replies

2,408 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Higgs_Boson 

You can use sys.attach command after any reset or after power-on to re-establish debug session without reset (copied from debugger_arm.pdf):

lukaszadrapa_0-1678806573781.png

After functional/destructive reset, the device boots from normal reset vector as usual. Startup files then contains code which initializes the RAM. 

Regards,

Lukas

0 Kudos
Reply

2,403 Views
Higgs_Boson
Contributor I

Hi, 

A Functional Reset will cause RAM content loss? How does "Self Test Done Functional Reset" / "Functional Reset" means.

 

Thanks.

0 Kudos
Reply

2,395 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Higgs_Boson 

generally, functional resets will keep SRAM data unchanged by hardware mechanism.
Destructive resets cannot guarantee the SRAM data integrity.

However, SRAM self test cannot keep the SRAM content. It's destructive operation.

Regards,

Lukas

 

0 Kudos
Reply