S32K3 AB Swap without HSE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 AB Swap without HSE

Jump to solution
6,981 Views
ValTek
Contributor III

Hi,

I'm looking for some clarification regarding the AB Swap functionality. Here the questions:

1. Is it possible to do an AB Swap without the HSE (only sBAF)? Or is HSE required? Is there some demo app for this?

2. Is it possible to change the size of the AB Swap blocks? For example on a S32K312 use only 128 KB (x2 256 KB) and than use the remaining space for other purposes? 

0 Kudos
Reply
1 Solution
6,898 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
3 Replies
6,899 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

0 Kudos
Reply
6,711 Views
PatrickPP
Contributor I

hi lucas,

Can you tell me that where can i download the SW32K3_OTADEMO_0.8.0_D2203?

thanks a lot.

0 Kudos
Reply
6,966 Views
ValTek
Contributor III

Hi, probably this is another reply...

0 Kudos
Reply