S32K3 AB Swap without HSE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 AB Swap without HSE

ソリューションへジャンプ
6,980件の閲覧回数
ValTek
Contributor III

Hi,

I'm looking for some clarification regarding the AB Swap functionality. Here the questions:

1. Is it possible to do an AB Swap without the HSE (only sBAF)? Or is HSE required? Is there some demo app for this?

2. Is it possible to change the size of the AB Swap blocks? For example on a S32K312 use only 128 KB (x2 256 KB) and than use the remaining space for other purposes? 

0 件の賞賛
返信
1 解決策
6,897件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
6,898件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

0 件の賞賛
返信
6,710件の閲覧回数
PatrickPP
Contributor I

hi lucas,

Can you tell me that where can i download the SW32K3_OTADEMO_0.8.0_D2203?

thanks a lot.

0 件の賞賛
返信
6,965件の閲覧回数
ValTek
Contributor III

Hi, probably this is another reply...

0 件の賞賛
返信