S32K3 AB Swap without HSE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 AB Swap without HSE

跳至解决方案
6,971 次查看
ValTek
Contributor III

Hi,

I'm looking for some clarification regarding the AB Swap functionality. Here the questions:

1. Is it possible to do an AB Swap without the HSE (only sBAF)? Or is HSE required? Is there some demo app for this?

2. Is it possible to change the size of the AB Swap blocks? For example on a S32K312 use only 128 KB (x2 256 KB) and than use the remaining space for other purposes? 

0 项奖励
回复
1 解答
6,888 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
3 回复数
6,889 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Vincenzo,

  1. No, AB Swap is supported only with HSE. You can download HSE FW and HSE demo app, HSE OTADEMO from S32K3 Standard Software and S32K3 Reference Software packages:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

  1. No, that’s not possible.

Regards,

Lukas

0 项奖励
回复
6,701 次查看
PatrickPP
Contributor I

hi lucas,

Can you tell me that where can i download the SW32K3_OTADEMO_0.8.0_D2203?

thanks a lot.

0 项奖励
回复
6,956 次查看
ValTek
Contributor III

Hi, probably this is another reply...

0 项奖励
回复