S32K1xx LPI2C RX Command Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K1xx LPI2C RX Command Question

2,545件の閲覧回数
stephen_humphre
Contributor II

I am implementing a driver for the S32K1xx family's LPI2C peripheral and am trying to understand the RX command behavior.  

For example, if I load the following set of commands into the TX FIFO:

  • CMD: 0x04 DATA: 0x55   (Generate START + Address)
  • CMD: 0x01 DATA: 255  (Receive 256 bytes)
  • CMD: 0x02 DATA: 0    (Generate STOP)

I then enable the RDF interrupt by setting MIER.RDIE to 1.

I then have an interrupt handler that handles processing the RDF event.  If I place a break point in the interrupt handler, based on what I read in the reference manual, I would expect to see four bytes get clocked in and then have the peripheral stall since the RX FIFO is full.  But what I am seeing on my scope is the break point hits but all 256 bytes are clocked on the SCL line.  This leads me to "missing" all of the bytes due to the breakpoint.  

I have MCR.DBGEN set to 1.

Any idea what the expected operation should be? 

 

0 件の賞賛
返信
3 返答(返信)

2,530件の閲覧回数
stephen_humphre
Contributor II

I wrote a little test code to try and understand the behavior of the LPI2C peripheral.  It does not use interrupts, but rather polls relevant flags:

stephen_humphre_0-1613143941957.pngstephen_humphre_0-1613143941957.png

If I simply put a break point at line 62 (at the end) this code runs fine and I receive two bytes.  But if I place a break point at line 28 where the peripheral is enabled and try and step through the code, I see the whole transfer appear on my scope, and I can step through the while loop that waits for RDF to get set at line 37, but the MRDR register just reads 0x00004000 (RX FIFO empty) and so my received byte counter never gets incremented and I am forever stuck in the while loop waiting for received bytes.

Any idea what is going on?  Is the debugger (S32DS) somehow pulling the received bytes out of the RXFIFO before my code can get to them?  I would expect when I hit the break point at line 28 and start stepping that at some point I would see RDF get set, see MFSR.RXCOUNT get to 2, and see the first value (without the RXEMPTY flag set) sitting in MRDR.  But with stepping, I never see any of that.  RDF always appears 0, RXCOUNT always 0, and RXEMPTY always 1.

I have tried this code with MCR.DBGEN both set and cleared.  The only difference when it is set is that the entire transfer appears when I do the first step after hitting the breakpoint at line 28, and I never make it past the while at line 37 that waits for the RDF flag to set.  

0 件の賞賛
返信

2,526件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please close the EmbSys Register view and the Memory view - everything that can read the data register.

 

Thank you,

BR, Daniel

 

0 件の賞賛
返信

2,538件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Stephen,

This is the expected operation.

If DBGEN == 1, the LPI2C module continuous operating.

 

Regards,

Daniel

 

0 件の賞賛
返信