S32K14x Program running Ram or Flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K14x Program running Ram or Flash?

1,567 次查看
1603279584
Contributor I

The s32k142,debug arm program that I use jlinkv9.4 debug can run normally, but after burning program should not burn to flash, the program does not run after I restart, this also has boot foot to choose where program starts to run? I didn't find it.

标签 (1)
0 项奖励
回复
1 回复

1,492 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport
Hi Yingkun,
Have you try to program the SDK examples?
I have try to test these examples. Did not see similar phenomenon on S32K142EVB.
If you are test your own project, would you please check if WDOG is enabled or feed WODG periodically.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复