S32K14x Program running Ram or Flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x Program running Ram or Flash?

1,117 Views
1603279584
Contributor I

The s32k142,debug arm program that I use jlinkv9.4 debug can run normally, but after burning program should not burn to flash, the program does not run after I restart, this also has boot foot to choose where program starts to run? I didn't find it.

Labels (1)
0 Kudos
Reply
1 Reply

1,042 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
Hi Yingkun,
Have you try to program the SDK examples?
I have try to test these examples. Did not see similar phenomenon on S32K142EVB.
If you are test your own project, would you please check if WDOG is enabled or feed WODG periodically.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply