S32K148 program download in STOP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148 program download in STOP mode

681 次查看
SONGTAOSI
Contributor I

Hi,

When I tested LPSPI wake up low power, I use LPSPI's Transfer complete interrupt wake up STOP1. However, due to configuration problems, the Transfer complete interrupt did not occur. When the chip was powered on, it went into STOP mode always, and I couldn't recognize the chip when I download new programs. How do I download new programs into chip.

Looking forward to your reply.

0 项奖励
回复
1 回复

669 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi SONGTAOSI,

See this article: Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power
You can find P&E Recovery Utility in: Can't use PEmicro debugger with S32K118EVB2-Q048


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复