S32K148 program download in STOP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 program download in STOP mode

705件の閲覧回数
SONGTAOSI
Contributor I

Hi,

When I tested LPSPI wake up low power, I use LPSPI's Transfer complete interrupt wake up STOP1. However, due to configuration problems, the Transfer complete interrupt did not occur. When the chip was powered on, it went into STOP mode always, and I couldn't recognize the chip when I download new programs. How do I download new programs into chip.

Looking forward to your reply.

0 件の賞賛
返信
1 返信

693件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi SONGTAOSI,

See this article: Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power
You can find P&E Recovery Utility in: Can't use PEmicro debugger with S32K118EVB2-Q048


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信