S32K148 + TJA1101 LWIP Client-Server example Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 + TJA1101 LWIP Client-Server example Project

3,590件の閲覧回数
ethan-li
Contributor III

Hi Guys,

   How can i get the LWIP Client-Server examples Projects based on S32K148+TJA1101 ? Or is there any document that introduce how to use LWIP example in S32 DS RTM3.0 SDK implement Client/Server Demo useing two S32K148+TJA1101 Boards?

0 件の賞賛
返信
2 返答(返信)

3,558件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Ethan,

A basic application that presents the lwIP usage is available in the S32DS -> File -> New -> S32DS Project from Example: lwip_s32k148

The example documentation can be found in the S32 SDK documentation which is located in the installation folder:

C:/NXP/S32DS_ARM_v2.2/S32DS/software/S32SDK_S32K1xx_RTM_3.0.0/doc/html_S32K148/lwip_s32k148_group.html 

Also, I suggest checking related community thread:

S32K148 lwip can not ping Ethernet 

I hope it helps.

Best regards,

Diana

0 件の賞賛
返信

3,558件の閲覧回数
ethan-li
Contributor III

Diana,

     thanks, I will try it based on these two examples in S32 DS SDK: LWIP_S32K148 & PHY_TJA1101_S32K148.

0 件の賞賛
返信