S32K148 SPI driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 SPI driver

8,779 Views
Saitej
Contributor IV

Hello NXP

Here am with S32K148 and using process expert configuration for spi and it is working fine as expected for my use case, but I have a situation where i need to do the spi transfer before the RTOS get started

In the situation am in need of blocking call, where I believe "SPI_MasterTransfer()" function from PAL drivers is not using any RTOS functions & if I use this function and a blocking loop for transaction to be completed in back ground, but cursor stay's in loop itself & IRQ function is never called and so call back function is never called.

Do we have any SPI driver without OS dependency, may be bare metal drivers. 

please do the needful.  

0 Kudos
Reply
15 Replies

8,746 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Saitej,

Sorry for my delay!
Have you tried to use S32SDK S32K1xx RTM 4.0.1? It did not use Processor Expert.

In addition, there is an bare metal example of SPI in S32K1xx development package. You need to install S32K1xx development package in S32 Design Studio for ARM Version 2.2.

S32K148_Project_LPSPI.pngS32K148_Project_LPSPI example.pngS32K1xx development package.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

8,744 Views
Saitej
Contributor IV

Hello @Robin_Shen 

Thanks for the replay , sorry for confusing with my wordings in previous post , actually here am already using PAL driver & they are serving my purpose, now am in situation where i need to reuse same drivers before RTOS get started right after PIN_DRV_INIT().

here below is my code snippet

static uint8_t TxData_au8[2U] = { 0x01, 0x02 };
static uint8_t RxData_au8[2u];
static boolean SPI_Transfer_CompFlag;
static void SBC_Test(void)
{
    SPI_MasterInit(&SPI_PERIInstance, &SPI_PERI_MasterConfig);
    INT_SYS_SetPriority(g_lpspiIrqId[SPI_PERIInstance.instIdx], 0);
     if(STATUS_SUCCESS == SPI_MasterTransfer(&SPI_PERIInstance,TxData_au8,RxData_au8,1))
     {
           while (false == SPI_Transfer_CompFlag);
            return RxData_au8;      
     }
}
void SPI1_TxRxTransferCompleteCB(void *driverState, spi_event_t event, void *userData)
{
SPI_Transfer_CompFlag = true;
}

The reason for using SPI_MasterTransfer() as a blocking call since it not using any RTOS functions, as you see in my code snippet it is working fine as expected when I set priority to 0 and for other priorities(default or 1) it won't coming to call back function.

below are the screen shots of the NVIC registers which says other interrupts are not set yet.

priority 0priority 0priority 1priority 1

 

0 Kudos
Reply

8,712 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The lower priority number, the higher priority level. But the value of NVIC shows there are no other interrupts.

Another strange thing is that why the value of IER SPI1 are different when just change priority 0 to priority 1.

0 Kudos
Reply

8,650 Views
Saitej
Contributor IV

@Robin_Shen 

do you have any other comments .. please help me out !

0 Kudos
Reply

8,707 Views
Saitej
Contributor IV

Hello @Robin_Shen 

That's my question even though I see same register contents by setting priority to 1 or 0, why only priority 0 is working.

0 Kudos
Reply

8,601 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry to keep you waiting!
I was on vacation recently and just back to the office.
Have you check the value of Interrupt Priority Register?
INT_SYS_SetPriority(LPSPI1_IRQn, 1); I can see the value be set in Interrupt Priority Register of LPSPI1.

INT_SYS_SetPriority(LPSPI1_IRQn, 1);.pngS32K1xx_DMA_Interrupt_mapping.png

Would you please attached the simplified test program? So that I can test directly. 

0 Kudos
Reply

8,583 Views
Vijay_Arwapally
Contributor III

@Robin_Shen 

I am not able to reproduce this issue with example project. But this happens with actual project that we are working on.

Below are content of SPI register and NVIC registers. SPI register have Interrupt enabled, and from NVIC as well, it is evident that interrupt (LPSPI1 i.e. IRQ 27 is pending) but still IRQ handler isnt invoked.

SPI Registers:

Vijay_Arwapally_0-1613642226113.png

Since the IER register content has interrupts enabled, as SR also indicates TDF bit set, which should trigger IRQ, but that doesnt happen, no clue why.

Status of NVIC registers at this point:

As shown below, IRQ 27 is enabled and is pending.

Vijay_Arwapally_1-1613642328529.png

Priority Registers:

Vijay_Arwapally_2-1613642389154.png

Vijay_Arwapally_3-1613642405380.png

 

Vijay_Arwapally_4-1613642418507.png

 

Vijay_Arwapally_5-1613642437424.png

 

Vijay_Arwapally_6-1613642448369.png

 

 

 

0 Kudos
Reply

8,546 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if you configure the BASEPRI 

BASEPRI.png

If you can send your project to me, it would be better to check issue.

 

 

0 Kudos
Reply

8,493 Views
Vijay_Arwapally
Contributor III

BASEPRI is not configured. Sharing the project may not be possible.

Vijay_Arwapally_0-1613972303872.png

 

0 Kudos
Reply

8,556 Views
Vijay_Arwapally
Contributor III

@Robin_Shen @nxp  Kindly expedite this issue ASAP. This issue is open since long time.

0 Kudos
Reply

8,671 Views
Saitej
Contributor IV

Hello @Robin_Shen 

are you able to replicate the situation ?

0 Kudos
Reply

8,702 Views
Saitej
Contributor IV

any update please 

0 Kudos
Reply

8,734 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you tried to use SPI_MasterTransferBlocking? This function initializes a blocking master transfer with time-out.

SPI_MasterTransferBlocking.png

0 Kudos
Reply

8,732 Views
Saitej
Contributor IV

Yes, story started over their , as TransferBlocking function call uses time out but here RTOS is not started yet so it throwing errors. 

I believe blocking call will not work before RTOS get started

0 Kudos
Reply

8,765 Views
Saitej
Contributor IV

@danielmartynek 

Any update

0 Kudos
Reply