S32K148 Input capture constant reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 Input capture constant reset

1,523件の閲覧回数
1462993357
Contributor I
  • PWM output:PTE20 FTM4_0
    Input capture:PTD13 FTM2_4
  • Connect two pins with dupont wire.

Test input capture with component [ftm_ic],The debug software keeps resetting. what is the reason.

It is normal to disconnect the DuPont line.

(マイビデオを表示)

タグ(1)
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi  ruide,

Have you refer the ftm_signal_measurement_s32k148 example?

ftm_signal_measurement_s32k148.png

FTM Signal Measurement.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信