S32K148 FlexRAM Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 FlexRAM Question

ソリューションへジャンプ
1,760件の閲覧回数
kmh48301
Contributor IV

Hi

 

1.

I need to know the value of FlexRAM area when it is delivered from NXP (Virgin Device)

[0x14000000 ~ 0x1400ffff]

Currently, I don't have the s32k148 virgin device. So I can't check the value.

(Random(garbage) Value or 0 or 1?)

 

2.

I have develepment board.

And I did "partition command" to this EVB for csec use.

And after I did "erase all command" to this EVB, FlexRAM area value became 0xFF.

Is this value moved from FlexNVM?

 

These are related to mass production project.

I'm looking forward to reply.

 

Thanks

Best Regards

Phillip

0 件の賞賛
返信
1 解決策
1,728件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1 返信
1,729件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I the past I made example code for this:

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K146-Set-whole-FlexRAM-as-RAM-v0-0-S32DS...

Pay attention to its description

0 件の賞賛
返信