S32K148 FlexRAM Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 FlexRAM Question

Jump to solution
1,816 Views
kmh48301
Contributor IV

Hi

 

1.

I need to know the value of FlexRAM area when it is delivered from NXP (Virgin Device)

[0x14000000 ~ 0x1400ffff]

Currently, I don't have the s32k148 virgin device. So I can't check the value.

(Random(garbage) Value or 0 or 1?)

 

2.

I have develepment board.

And I did "partition command" to this EVB for csec use.

And after I did "erase all command" to this EVB, FlexRAM area value became 0xFF.

Is this value moved from FlexNVM?

 

These are related to mass production project.

I'm looking forward to reply.

 

Thanks

Best Regards

Phillip

0 Kudos
Reply
1 Solution
1,784 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
1 Reply
1,785 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I the past I made example code for this:

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K146-Set-whole-FlexRAM-as-RAM-v0-0-S32DS...

Pay attention to its description

0 Kudos
Reply