S32K146 WDOG_EWM_IRQHandler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 WDOG_EWM_IRQHandler

Jump to solution
1,682 Views
DarrenD
Contributor III

How do I enable the WDOG_EWM_IRQHandler?

I thought I only needed to set WDOG.CS[INT] = 1 and enable NVIC entry 22 (WDOG_EWM_IRQn) to force a call to WDOG_EWM_IRQHandler whenever WDOG.CNT reaches WDOG.TOVAL to allow me to do some tidy up code before the CPU resets 128 bus clock cycles later. This comes from reading 23.1.4 Watchdog Timeout Reaction

I am using an S32K146EVB-Q144 dev board running at 80MHz

My WDOG settings are (21us watchdog using 8MHz SIRC)
WDOG.WIN = 0
WDOG.TOVAL = 168
WDOG.CS = 0x27E0 (UPDATE=1, INT=1, EN=1, CLK=3, RCS=1, CMD32EN=1)

My NVIC settings are
S32_NVIC.ISER[0] = 0x0040_0000 (bit 22 set)
S32_NVIC.ISPR[0] = 0x0000_0000
S32_NVIC.IP[22] = 16 (priority = 1)

I have interrupts enabled
General Regsiters -> primask = 0
General Regsiters -> basepri = 0

I have my void WDOG_EWM_IRQHandler(void) code written with a breakpoint on the first line of code

I ran some wait loop code while WDOG.CNT < 160 and then stopped at a breakpoint. I then single-stepped on a few instructions via the OpenSDA debugger on my dev board and monitor WDOG.CNT incrementing towards 168 (I saw 166) and then it reset to Reset_Handler. I do not see WDOG.CS change to show FLG=1, nor the interrupt firing

What am I missing?
Thanks
Darren

0 Kudos
Reply
1 Solution
1,602 Views
DarrenD
Contributor III

Hopefully this explanation below will help others.

 

Thanks for the example code; it helped a lot. My handler code was being executed but the debugger does not halt at a breakpoint in the WDOG_EWM_IRQHandler. I think this is down to the way the WDOG resets the CPU after the 128 bus cycles that the debugger cannot prevent.

The example code is difficult to see working since the IRQ handler toggles an LED rapidly for about 4ms and then the reset happens so the LED turns off.

 

I have modified the example code (after changing S32K144 references to S32K146) to add some variables. Inserting a breakpoint at the start of Reset_Handler, i.e. before C variables are initialised allowed me to see the values that these variables reached after the previous CPU reset.

I changed RCM_WSDOG_INT to 0 (so the code uses WDOG_EWM_IRQHandler and not RCM_IRQHandler).

I added the following variables at the top of main.c

int wdog_called;
int wdog_cs;
int wdog_detected;
int wdog_loop;

int main_loop;

I modified the "WDOG_EWM_IRQHandler" function (my additions start with /**/ comment)

void WDOG_EWM_IRQHandler(void)
{
/**/wdog_called++;
/**/wdog_cs = WDOG->CS;
    if(WDOG->CS & 0x4000)           // [14] FLG Watchdog Interrupt Flag
    {
/**/    wdog_detected++;
        // WDOG->CS |= 0x4000;      // Clear the flag
        while(1)
        {
/**/        wdog_loop++;
            PTD->PTOR |= (1 << 15); // Toggle RED LED until reset
        }
    }
}

I modified the "main" function (my additions start with /**/ comment)

...
    while(1)
    {
/**/    main_loop++;
    }
...

I then set the breakpoint on the start of the Reset_Handler function

I then programmed the dev board and it stopped at "main" (part of the debug configuration settings)

I created watch expressions for my variables

I then pressed F8 (run) and the debugger halted at Reset_Handler at which point I could see the following values

wdog_called   int 1
wdog_cs       int 0x65e0 (Hex)
wdog_detected int 1
wdog_loop     int 142
main_loop     int 2096993

This was the proof that WDOG_EWM_IRQHandler was being called. Note 0x65e0 includes 0x4000 (the FLG bit)

I then put a breakpoint on the "wdog_detected++;" line and ran again

The debugger halted at Reset_Handler and I got the following values

wdog_called   int 1	
wdog_cs       int 0x65e0 (Hex)	
wdog_detected int 0	
wdog_loop     int 0	
main_loop     int 2097011	

This was the proof that WDOG_EWM_IRQHandler was being called and that the debugger tried to stop at the "wdog_detected++;" line but could not get control of the CPU before the WDOG reset the CPU. This failure to stop at any breakpoint in WDOG_EWM_IRQHandler was why I originally thought it was not executing my WDOG_EWM_IRQHandler.

View solution in original post

0 Kudos
Reply
2 Replies
1,655 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @DarrenD 

You can refer to the example in the thread Example S32K144 WDOG RCM Interrupt. It should give you a good reference for your application.

 

BR, VaneB

1,603 Views
DarrenD
Contributor III

Hopefully this explanation below will help others.

 

Thanks for the example code; it helped a lot. My handler code was being executed but the debugger does not halt at a breakpoint in the WDOG_EWM_IRQHandler. I think this is down to the way the WDOG resets the CPU after the 128 bus cycles that the debugger cannot prevent.

The example code is difficult to see working since the IRQ handler toggles an LED rapidly for about 4ms and then the reset happens so the LED turns off.

 

I have modified the example code (after changing S32K144 references to S32K146) to add some variables. Inserting a breakpoint at the start of Reset_Handler, i.e. before C variables are initialised allowed me to see the values that these variables reached after the previous CPU reset.

I changed RCM_WSDOG_INT to 0 (so the code uses WDOG_EWM_IRQHandler and not RCM_IRQHandler).

I added the following variables at the top of main.c

int wdog_called;
int wdog_cs;
int wdog_detected;
int wdog_loop;

int main_loop;

I modified the "WDOG_EWM_IRQHandler" function (my additions start with /**/ comment)

void WDOG_EWM_IRQHandler(void)
{
/**/wdog_called++;
/**/wdog_cs = WDOG->CS;
    if(WDOG->CS & 0x4000)           // [14] FLG Watchdog Interrupt Flag
    {
/**/    wdog_detected++;
        // WDOG->CS |= 0x4000;      // Clear the flag
        while(1)
        {
/**/        wdog_loop++;
            PTD->PTOR |= (1 << 15); // Toggle RED LED until reset
        }
    }
}

I modified the "main" function (my additions start with /**/ comment)

...
    while(1)
    {
/**/    main_loop++;
    }
...

I then set the breakpoint on the start of the Reset_Handler function

I then programmed the dev board and it stopped at "main" (part of the debug configuration settings)

I created watch expressions for my variables

I then pressed F8 (run) and the debugger halted at Reset_Handler at which point I could see the following values

wdog_called   int 1
wdog_cs       int 0x65e0 (Hex)
wdog_detected int 1
wdog_loop     int 142
main_loop     int 2096993

This was the proof that WDOG_EWM_IRQHandler was being called. Note 0x65e0 includes 0x4000 (the FLG bit)

I then put a breakpoint on the "wdog_detected++;" line and ran again

The debugger halted at Reset_Handler and I got the following values

wdog_called   int 1	
wdog_cs       int 0x65e0 (Hex)	
wdog_detected int 0	
wdog_loop     int 0	
main_loop     int 2097011	

This was the proof that WDOG_EWM_IRQHandler was being called and that the debugger tried to stop at the "wdog_detected++;" line but could not get control of the CPU before the WDOG reset the CPU. This failure to stop at any breakpoint in WDOG_EWM_IRQHandler was why I originally thought it was not executing my WDOG_EWM_IRQHandler.

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2259327%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ES32K146%20WDOG_EWM_IRQHandler%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2259327%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHow%20do%20I%20enable%20the%20WDOG_EWM_IRQHandler%3F%3C%2FP%3E%3CP%3EI%20thought%20I%20only%20needed%20to%20set%20WDOG.CS%5BINT%5D%20%3D%201%20and%20enable%20NVIC%20entry%2022%20(WDOG_EWM_IRQn)%20to%20force%20a%20call%20to%20WDOG_EWM_IRQHandler%20whenever%20WDOG.CNT%20reaches%20WDOG.TOVAL%20to%20allow%20me%20to%20do%20some%20tidy%20up%20code%20before%20the%20CPU%20resets%20128%20bus%20clock%20cycles%20later.%20This%20comes%20from%20reading%2023.1.4%20Watchdog%20Timeout%20Reaction%3C%2FP%3E%3CP%3EI%20am%20using%20an%20S32K146EVB-Q144%20dev%20board%20running%20at%2080MHz%3C%2FP%3E%3CP%3EMy%20WDOG%20settings%20are%20(21us%20watchdog%20using%208MHz%20SIRC)%3CBR%20%2F%3EWDOG.WIN%20%3D%200%3CBR%20%2F%3EWDOG.TOVAL%20%3D%20168%3CBR%20%2F%3EWDOG.CS%20%3D%200x27E0%20(UPDATE%3D1%2C%20INT%3D1%2C%20EN%3D1%2C%20CLK%3D3%2C%20RCS%3D1%2C%20CMD32EN%3D1)%3C%2FP%3E%3CP%3EMy%20NVIC%20settings%20are%3CBR%20%2F%3ES32_NVIC.ISER%5B0%5D%20%3D%200x0040_0000%20(bit%2022%20set)%3CBR%20%2F%3ES32_NVIC.ISPR%5B0%5D%20%3D%200x0000_0000%3CBR%20%2F%3ES32_NVIC.IP%5B22%5D%20%3D%2016%20(priority%20%3D%201)%3C%2FP%3E%3CP%3EI%20have%20interrupts%20enabled%3CBR%20%2F%3EGeneral%20Regsiters%20-%26gt%3B%20primask%20%3D%200%3CBR%20%2F%3EGeneral%20Regsiters%20-%26gt%3B%20basepri%20%3D%200%3C%2FP%3E%3CP%3EI%20have%20my%20void%20WDOG_EWM_IRQHandler(void)%20code%20written%20with%20a%20breakpoint%20on%20the%20first%20line%20of%20code%3C%2FP%3E%3CP%3EI%20ran%20some%20wait%20loop%20code%20while%20WDOG.CNT%20%26lt%3B%20160%20and%20then%20stopped%20at%20a%20breakpoint.%20I%20then%20single-stepped%20on%20a%20few%20instructions%20via%20the%20OpenSDA%20debugger%20on%20my%20dev%20board%20and%20monitor%20WDOG.CNT%20incrementing%20towards%20168%20(I%20saw%20166)%20and%20then%20it%20reset%20to%20Reset_Handler.%20I%20do%20not%20see%20WDOG.CS%20change%20to%20show%20FLG%3D1%2C%20nor%20the%20interrupt%20firing%3C%2FP%3E%3CP%3EWhat%20am%20I%20missing%3F%3CBR%20%2F%3EThanks%3CBR%20%2F%3EDarren%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2259477%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20S32K146%20WDOG_EWM_IRQHandler%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2259477%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F201492%22%20target%3D%22_blank%22%3E%40DarrenD%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EYou%20can%20refer%20to%20the%20example%20in%20the%20thread%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32K-Knowledge-Base%2FExample-S32K144-WDOG-RCM-interrupt%2Fta-p%2F1107039%22%20target%3D%22_blank%22%3EExample%20S32K144%20WDOG%20RCM%20Interrupt%3C%2FA%3E.%20It%20should%20give%20you%20a%20good%20reference%20for%20your%20application.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EBR%2C%20VaneB%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2260419%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20S32K146%20WDOG_EWM_IRQHandler%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2260419%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHopefully%20this%20explanation%20below%20will%20help%20others.%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EThanks%20for%20the%20example%20code%3B%20it%20helped%20a%20lot.%26nbsp%3B%3CSPAN%3EMy%20handler%20code%20was%20being%20executed%20but%20the%20debugger%20does%20not%20halt%20at%20a%20breakpoint%20in%20the%26nbsp%3BWDOG_EWM_IRQHandler.%20I%20think%20this%20is%20down%20to%20the%20way%20the%20WDOG%20resets%20the%20CPU%20after%20the%20128%20bus%20cycles%20that%20the%20debugger%20cannot%20prevent.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3EThe%20example%20code%20is%20difficult%20to%20see%20working%20since%20the%20IRQ%20handler%20toggles%20an%20LED%20rapidly%20for%20about%204ms%20and%20then%20the%20reset%20happens%20so%20the%20LED%20turns%20off.%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%3CSPAN%3EI%20have%20modified%20the%20example%20code%20(after%20changing%20S32K144%20references%20to%20S32K146)%20to%20add%20some%20variables.%20Inserting%20a%20breakpoint%20at%20the%20start%20of%20Reset_Handler%2C%20i.e.%20before%20C%20variables%20are%20initialised%20allowed%20me%20to%20see%20the%20values%20that%20these%20variables%20reached%20after%20the%20previous%20CPU%20reset.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3EI%20changed%20RCM_WSDOG_INT%20to%200%20(so%20the%20code%20uses%26nbsp%3BWDOG_EWM_IRQHandler%20and%20not%26nbsp%3BRCM_IRQHandler).%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3EI%20added%20the%20following%20variables%20at%20the%20top%20of%20main.c%3C%2FSPAN%3E%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%3Eint%20wdog_called%3B%0Aint%20wdog_cs%3B%0Aint%20wdog_detected%3B%0Aint%20wdog_loop%3B%0A%0Aint%20main_loop%3B%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EI%20modified%20the%20%22WDOG_EWM_IRQHandler%22%20function%20(my%20additions%20start%20with%20%2F**%2F%20comment)%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%3Evoid%20WDOG_EWM_IRQHandler(void)%0A%7B%0A%2F**%2Fwdog_called%2B%2B%3B%0A%2F**%2Fwdog_cs%20%3D%20WDOG-%26gt%3BCS%3B%0A%20%20%20%20if(WDOG-%26gt%3BCS%20%26amp%3B%200x4000)%20%20%20%20%20%20%20%20%20%20%20%2F%2F%20%5B14%5D%20FLG%20Watchdog%20Interrupt%20Flag%0A%20%20%20%20%7B%0A%2F**%2F%20%20%20%20wdog_detected%2B%2B%3B%0A%20%20%20%20%20%20%20%20%2F%2F%20WDOG-%26gt%3BCS%20%7C%3D%200x4000%3B%20%20%20%20%20%20%2F%2F%20Clear%20the%20flag%0A%20%20%20%20%20%20%20%20while(1)%0A%20%20%20%20%20%20%20%20%7B%0A%2F**%2F%20%20%20%20%20%20%20%20wdog_loop%2B%2B%3B%0A%20%20%20%20%20%20%20%20%20%20%20%20PTD-%26gt%3BPTOR%20%7C%3D%20(1%20%26lt%3B%26lt%3B%2015)%3B%20%2F%2F%20Toggle%20RED%20LED%20until%20reset%0A%20%20%20%20%20%20%20%20%7D%0A%20%20%20%20%7D%0A%7D%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EI%20modified%20the%20%22main%22%20function%20(my%20additions%20start%20with%20%2F**%2F%20comment)%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%3E...%0A%20%20%20%20while(1)%0A%20%20%20%20%7B%0A%2F**%2F%20%20%20%20main_loop%2B%2B%3B%0A%20%20%20%20%7D%0A...%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EI%20then%20set%20the%20breakpoint%20on%20the%20start%20of%20the%26nbsp%3B%3CSPAN%3EReset_Handler%20function%3C%2FSPAN%3E%3C%2FP%3E%3CP%3EI%20then%20programmed%20the%20dev%20board%20and%20it%20stopped%20at%20%22main%22%20(part%20of%20the%20debug%20configuration%20settings)%3C%2FP%3E%3CP%3EI%20created%20watch%20expressions%20for%20my%20variables%3C%2FP%3E%3CP%3EI%20then%20pressed%20F8%20(run)%20and%20the%20debugger%20halted%20at%20Reset_Handler%20at%20which%20point%20I%20could%20see%20the%20following%20values%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%3Ewdog_called%20%20%20int%201%0Awdog_cs%20%20%20%20%20%20%20int%200x65e0%20(Hex)%0Awdog_detected%20int%201%0Awdog_loop%20%20%20%20%20int%20142%0Amain_loop%20%20%20%20%20int%202096993%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EThis%20was%20the%20proof%20that%26nbsp%3BWDOG_EWM_IRQHandler%20was%20being%20called.%20Note%200x65e0%20includes%200x4000%20(the%20FLG%20bit)%3C%2FP%3E%3CP%3EI%20then%20put%20a%20breakpoint%20on%20the%20%22wdog_detected%2B%2B%3B%22%20line%20and%20ran%20again%3C%2FP%3E%3CP%3EThe%20debugger%20halted%20at%20Reset_Handler%20and%20I%20got%20the%20following%20values%3C%2FP%3E%3CPRE%20class%3D%22lia-code-sample%20language-c%22%3E%3CCODE%3Ewdog_called%20%20%20int%201%09%0Awdog_cs%20%20%20%20%20%20%20int%200x65e0%20(Hex)%09%0Awdog_detected%20int%200%09%0Awdog_loop%20%20%20%20%20int%200%09%0Amain_loop%20%20%20%20%20int%202097011%09%3C%2FCODE%3E%3C%2FPRE%3E%3CP%3EThis%20was%20the%20proof%20that%26nbsp%3BWDOG_EWM_IRQHandler%20was%20being%20called%20and%20that%20the%20debugger%20tried%20to%20stop%20at%20the%20%22wdog_detected%2B%2B%3B%22%20line%20but%20could%20not%20get%20control%20of%20the%20CPU%20before%20the%20WDOG%20reset%20the%20CPU.%20This%20failure%20to%20stop%20at%20any%20breakpoint%20in%26nbsp%3BWDOG_EWM_IRQHandler%20was%20why%20I%20originally%20thought%20it%20was%20not%20executing%26nbsp%3Bmy%26nbsp%3BWDOG_EWM_IRQHandler.%3C%2FP%3E%3C%2FLINGO-BODY%3E