S32K146 LPO clock source select

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 LPO clock source select

Jump to solution
2,052 Views
ZhaozhangChen
Contributor I

Hi

    I use the default LPO clock 128Khz in the BootLoader, but I need to use LPO clock 1Khz in the APP, but when I set LPO clock 1Khz when the BootLoader jumps to the APP, it does not take effect.The value of LPOCLKSEL register is 00b. Is there any way to set LPO to 1KHz in app.

ZhaozhangChen_0-1665219450690.pngZhaozhangChen_1-1665219497269.png

 

0 Kudos
Reply
1 Solution
2,042 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

View solution in original post

0 Kudos
Reply
1 Reply
2,043 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

0 Kudos
Reply